Other Parts Discussed in Thread: UCD9248
Hi,
I found that PTD08D210 is generating a voltage of 5.9V even when the UCD9248 is not configured. PTD08D210 has two power output and this problem is seen only in one channel, I even erased the UCD Flasmemory and confirmed that no PWM is going to PTD08D210 but still i see 5.9V in one of the channel.
Note: My evel board has 4 PTD08D210 which means 8 o/p voltage channels and 2 UCD9248 to control it , out of which in only one channel i have this problem. Is it the problem with the PTD08D210 , it was working fine only suddenly in one day this problem happened.