Other Parts Discussed in Thread: CC2640, , TPS61070, TPS61099, TPS61220
Hi,
I have made a design based on battery cell CR1632 3V to power CC2640 circuit with other comment. The design needs a voltage of 3V and maximum current of 50mA. I have created a circuit with tlv61225 (I used the same reference circuit proposed on datasheet)to power this board, but I can get working properly as I switch on to power this board the voltage drops from 3V to 1.8V which is not enough to power the board.
Is this circuit can draw 50mA with it at 3V? If not is there any other part that can be used with a coin cell battery to power a board with 3V -50mA or more relaxed 3V 100mA?
In the TI web site there is these circuit available TPS61070 and TPS61099, are they a good condidate for a coin cell?
Many thanks
Best regards,
Mourad