This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM82813: When will TPSM82813 be in full production?

Part Number: TPSM82813

Hi,

I have two questions about TPSM82813:

1. Why is the orderable part # XPSM82813SILT not TPSM82813SILT? Is that because it is the part # for samples only?

2. When will the part be in full production? Will the part # will be TPSM82813SILT for full production?

Thanks

Yong

  • Hi Yong,

    The TPSM82813 is on the web and sampling under the XPSM part number.  These samples can be used for prototype builds, etc.  At release, the orderable part number will be TPSM82813SILR.

    If you have a specific need date for a specific production ramp, please send me a private message to discuss those details.