Hello I am working with a BMS design Project using bq76PL455A-Q1 ,I just want to initialize the registers of bq76PL455A-Q1 device as a first step of my hardware test .I just make a small PCB board test for it by adding other components on the bread board just to get access to the IC and make sure how it works with the main Processor.
1.I don't know if I have to connect the UART interface to my main Micro controller or I can use the bq76PL455A-Q1 GUI by just using an RS232 to USB converter to my PC?
2.Shall I connect all the Sense pins or I can just get access to the registers without reading any voltages?
3.By using an external power using your reference design,I have to use 12 V with my signal generator?
Thank you in advance