Hello,
Question 1:
Refering to the BQ76920EVM on page 36, you can see a schematic circuit about the BQ7692000PW. My question is about the components: D1, D6, C17 and C18. What is the purpose of them?
Do they protect the circuit about overvoltage? Would it be okay, if I would not use this part of the circuit?
Question 2:
The TS1 Pin of the BQ7692000PW has two fuctions: It should measure the voltage and with this pin we are able to boot up the monitor-IC. Why are you using a 3k resistor at R22 ( Refering to the BQ76920EVM on page 36)
Is there a reason why you are using the voltage of the cell 1 "C1" to provide the TS1 with power?