Dear All,
I am using BQ24092 charger IC to charge my battery (Li-ion,3.7v,1800mAh). When i switch on the 5v to charge the battery, Charger IC is getting heated up like anything.
I have used thermal pad beneath the IC in my PCB board to protect from the heat but i am not successfull .It takes nearly 6hrs to charge from 0v to 3.8v, but as per the datasheet it should be less than 3hrs. Please help in this situation,
Details of the charger IC and circuit are as follows:
O/p voltage and current from charger IC is: 4.04v and 800mA
ISET resister used is: 680ohm.
preterm resistor used: 2K ohm
TS resistor used: 10K
Regards,
Rimpul