Greetings. Looking for a single cell Li-Ion battery charger capable of sensing a USB port's configuration to determine if 100/500/1500 (or 1800) mA can be drawn from the port without the assistance of an additional microcontroller. Something similar to the bq24050 but with the capability of reaching the 1.5/1.8A charge current mark. The bq24160 also offers close functionality, but I don't need a switching topology and I'd like to have sensing to hit the 500mA mark (seems like the 24160 jumps right from 100mA to 1500mA. Power path management would be a nice to have feature, but not a necessity. It seems like this would be a device that TI would carry, but I am not finding it. Any help would be greatly appreciated.