Rode recommended in the datasheet Bq24650 only adjusting the current to 8 A and the battery voltage to 13.8 V circuit.
Use a power set at 16 V laboratory to simulate the photovoltaic panel.
The LED pin 3 is connected STAT1 indicating load process however there is no battery connected.
I would like to better understand the interção pins REGN, PH, LODRV, HIDRV and BTST as the technical document is not clear interaction of these pins.
when connecting the battery nothing happens .... below are some images of measurements that realizaei in each ICpin relative to GND.
pin 1
pin2
pin 3
pin 4
pin 5
pin 6
pin 7
pin 8 without battery
pin 9
pin 10
pin 11
pin 12
pin 13
pin14
pin 15
pin 16
photo mounted below the circuit
if someone can help me thank .....