Hi,
We've been using the BQ24055 with a number of cells and recently encountered an issue relating to deep discharge condition.
If the cell becomes deeply discharged, the PCM on the battery pack kicks in in undervoltage at around 2.5V. After this event, is is not possible to revive and re-charge the cell using BQ24055 - the pack must be removed from the assembly and revived (carefully) using a power supply by applying ~3V with limited current. After reviving the pack (PCM allows connection again), it can be charged with the BQ24055 as normal.
This does not appear to be an issue with all packs, and is presumably an interaction between the PCM and the BQ24055. Are there any suggested methods to revive a deeply discharged cell with the BQ24055 in circuit?