Hello,
I am using the bq25504 as PV harvester with several PV cells in order to charge a 4.1V, 50uAh solid state rechargeable battery.
The issue I am dealing with is that when using a double PV cell with VIN_DC=1.08V and total cell power @1000 lux 145.0uW the bq25504 harvester is able to charge the battery (over night charge) and keep my system up and running for more than 2 hours in dark conditions.
However, when trying a more efficient single PV cell with VIN_DC=0.63V and total cell power @1000 lux 233.0uW with the same over night charge as above the my system is not running for more than 20minutes in darkness.
1) Is this has to do with the efficiency of the bq25504 ? (since the VIN_DC varies from 1.2V in the double PV cell case to the 0.63V in the single PV cell case)
2) How can I perform bq25504 efficiency calculations? (based on measured data)
Many Thanks
Nik