Wenjia-san,
Thank you for your continuous support towards the inquiry regarding bq24250 from our customer.
In addition to the inquiry regarding charge status on bq24250, I have some additional inquiries regarding TCOLD Fault on bq24250 from them.
Please refer to the items below, and feedback us with your comment.
On this inquiry, they are evaluating their own prototype with another battery which NTC Beta is 3435 degK.
This means that they changed the resistors value around TS pin from EVM as, R5=5.1kohm and R6=10kohm.
Also, this prototype could be connected to USB Interface Adaptor to control from GUI.
On this configuration, they found TCOLD Fault on GUI when battery plugged-in. This issue could be found occasionally, not depending on battery charged level.
On this case, the LED is turned on, but never turned off again (For more than 12 hours).
Also, we tried to do CE toggle from GUI and connecting CE pin to GND. However, this issue could not be resolved.
We assume that we need to add capacitor in parallel with R6 to absorb noise which is caused on plugging-in.
On this case, please let us clarify which capacitance would be suitable.
We thank you once again for your information.
Best regards,