Hi,
In testing the BQ25570 EVM these are the problems & doubts that remain,can any one help me in these:
- Vbias value (TP7 on board) is always oscillating around 10-20mv and it is not maintained at 1.2v according to datasheet. So due to this Vbat_uv is set to 0v approximately and when input Solar power is switched OFF, Vbat getting discharged to almost 0v (with in few minutes).But Vbat_ok toggling at 3v.Is this the problem of board?
- When input power is turned OFF: C_store, vbat also decreasing.(But according to the working of BQ25570 EVM as Cstore voltage decreases below v_uv ,connection between Vbat and C_store should be turned OFF so that vbat is maintained.)
- How vbias=1.2v internally generated on board?
- No much difference of toggling of bat_ok,prog_ok is observed as vbat_ok toggling at 3v both in charging case, discharging case.(But according to datasheet vbat_ok should toggle at vbatok_hyst=2.79v,vbatok_prog=2.99v,which is not happening)
- How MPPT 50%,80%(given connecting ) achieved using given resistor dividers on board (as only 75% can be possible with given resistor values of 5M,10M,5M ohms)?
- How can 80% be achieved by tying VOC_SAMP to VSTOR?
- Measured Vmpp,VRdiv,V_uv,V_ov are showing in tens of mv(different from required values), why?
Thank you.