HI
Could i check if there are any guidelines on the selection of Secondary storage elements(SSE)?
For example, there are several voltage rating for super cap.
If we would to select Vbatt_OV to 4.2, would a super cap with rated voltage of 4 , 4.2 or 4.5 work better.
DOes it make sense for to use a super cap rated at 6.3V but we will not be able to charge up (Vstor max is 5.5V)?
Which voltage rating is more sensible?
Like to zoom down on Typical application on 8.2.1
The design goals stated :
"VBAT_OK = 2.39 V, VBAT_OK_HYST = 2.80 V"
On figure 21, the Vbatt_ok starts following Vstor at around 3.2V. which is correct?
Ivan