Hi,
We are using the BQ24295, but we would like to know that while in buck and charging mode, how much output voltage we get on PMID and SYS pin while providing 5V input supply.
Regards,
Mrudang
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thanks for the solving the query.
Regards,
Mrudang
Regarding 1 and 2, Q1 is turned off.
Regarding 3, yes but keep in mind that the input current limit feature is controlled through Q1 so any current pulled through PMID will not be available to the system or to charge the battery.
Regarding 4, bq24296 does not have D+/D- but its boost output is from VBUS not PMID. If you don't want to use D+/D-, shorting D+=D- gives ILIM at startup = 1.5A while putting 15kohm to ground on each gives ILIM at startup=0.5A. Once the host is up and running, you can change ILIM.
Hi Jeff,
Thanks for support.
Please see my requirement as below.
I am working on Li-Ion battery battery charger.
My Input is 5V@500mA (USB Power). My system Load is 5V @ 200mA max. And I have 10AHr or 20AHr battery for charging. And I want both Buck and Boost output from single pin out (PMID).
I know charging process will be slow.
Please provide your valuable feedback.
Regards,
Mrudang
Hi Jeff,
Thanks for the support,
As I have told you. I have 5V@500mA USB power but i don't have any D-/D+ pin for input current limit.
Please find my charging circuit attached along with query.
Kindly provide your valuable feedback.
Please let me know if any other changes required for both Buck and Boost output from single pinout (PMID)..
Hi Jeff,
Thanks for your Valuable feedback.
Here I am attaching my circuit for verification from your end (TI's Expert Review).
My circuit contains both battery charging and battery monitoring circuit.
Kindly provide your valuable feedback with comments if I have missed any.