Based on the datasheet it sounds like the BQ25896 regulates VSYS to always be above 3.5V. The datasheet does not always explicitly state that the V_SYS_MIN =3.5 only applies for when external power is present, so I am a bit confused as to what is really the case, but based on my testing and what I found on this forum, V_SYS_MIN = 3.5 only applies when external power is present. Otherwise it will follow the battery voltage.
If this is truly the case, is there another battery charger that has a switching regulator built in that will keep V_SYS above 3.5V (or similar) even when run only off the battery?
My current design uses a TPS6300x buck/boost converter to generate a stable 3.3V at all times, but I'd like to consolidate to a simpler architecture with only a single IC.
Any suggestions are welcome.