Hi,
this is my first time use BQ24050, charging current is small because the batter capacity is small, 10mA based on my calculation, will this design work. if the VIN connect to load regulator, it will keep on during the charging. once charging complete. based on the current of this load, for example, 1mA on average. will BQ24050 keep output current, or it will shut down based on the battery is full.
Thanks,