Hello, I have a battery charger that we are producing and i am seeing higher than expected failure rates of the charging circuit. The circuit is powered by a 15V SMPS, uses at BQ24725A with a PIC18F25K22 micro to talk to a 12.6V Li-ion battery that uses a BQ3060 GG chip. In production we do a quick functional test of the circuit board and we are finding 5+% failure rate. The failure is that the circuit will not charge. From my testing, it appears that the PIC18F25K22 is correctly requesting charger voltage and current from the BQ24725A, but the chip is not able to provide charge current. I have been reviewing boards and it appears that i have potentially two failures 1. The BQ24725A chip itself or 2. Q2 transistor (as listed in the EVM for this chip). My circuit for the charge is almost identical to the EVM schematic and i use the same transistor for Q1 and Q2 as the EVM. I am concerned that there is some input transient voltage spike that is damaging either Q2 or the BQ24725A. I have a TVS on the input and the RC filter as well. Originally the TVS was a 36V clamping part, but i have changed this to a 18V clamping part and still seeing similar failures. (Q2 is a 30V Vds part). Does anyone have suggestions on how i can track down what is causing these failures?
Thanks Nathan