Team-
We have a customer that is trying to assess the failure mode/rate of the bq25892, specifically the Q2, Q4 FETs.
If these FETs were to both fail short, it could potentially connect the battery to Vbus.
Given that Q2 is driven off the SW node by the high side driver, I believe that it is a completely isolated from Q4, please confirm.
In this case, Vbus = 5V, and the cell is a 3.1A-hr Li-ion.
Additionally, they would like to know the locations of these FETs on the die- a micrograph would be helpful.
We have an NDA with this customer, so please contact me privately if needed to close out this thread.
Thanks, Best, S. Dunbar, AFA Colorado