Hi,
I've seen others having the same problem regarding Shipmode: if the charger reports Fault, Shipmode cannot be entered!
In our application this happens when we remove our external source. During this, the charger reports VIN_UV (and STAT_0, STAT_1 = 11). Unfortunately, there seems to be a mechanism inside BQ25120 that prevents the chip to go into Shipmode as long as a Fault is present.
We enter Shipmode by writing 0x20 to register 0x00. This works fine as long as there are no faults. Faults occur when the input voltage is slowly decreasing - even when reaching 0V the fault is still present.
My questions:
is there a way to clear the Fault without having to manually plug/unplug a power source?
or best, can we force Shipmode?
Ole