Other Parts Discussed in Thread: BQ2000EVM
Hi,
I have assembled the circuit as given in datasheet.
I need to charge 4NiMh batteries, accordingly I have changed the values of RB1 and RB2.
RB1 = 600KOhm And RB2 = 200KOhm
Instead of thermistor I have connected 10KOhm resistor.
The IC remains in Charge qualification or suspended state. LED flashes continuously at 1Hz rate.
Voltage at BAT= 0.7361 continuously.
It does not enter Fast charge state.
Please suggest what changes are required.