Other Parts Discussed in Thread: BQ24075, BQ24081-Q1, BQ21040, BQ24081
Hello,
Customer use below formula to calculate.
thermistor of customer ( 0~45 ° C temp. range)
RTH&RTC of spec.
RTH: 4924 Ω (resistance of 45 ° C )
RTC: 26490 Ω (resistance of 0 ° C )
VH: IC's Hot Trip Threshold = 0.3V nominal
VC: IC's Cold Trip Threshold = 2.1V nominal
ITS: IC's Output Current Bias = 75μA nominal
Use below formula to calculate RS. The results are -979 Ω &-30434Ω. What are correct RS value to select?
Another question, if use RP formula and datasheet thermistor spec.to calculate based on red mark value on below table, we still can't calculate right RP value as table 845000. Do you have any suggestion?
BR
Patrick