Hi, All:
I am using BQ24250M with Stand alone mode. when I start up with external 5V power ( don't insert the battery ),
BQ24250M will in battery detection status, the Vsys output voltage will be instable like below waveform( the VPP is about 1V, and the frequency will be 15Hz), This voltage will be the source voltage of the system and It will afftect system audio feature( have noise when recording audio), if we disable the charge function with /CE , the voltage is stable and the audio noise will disappear. Do you have any suggestions?
Thanks
Tiper Liu