Hello:
Now I am using BQ24175 for charging the 2S battery. But I don't know which method I use to terminate the charge cycle when battery voltage is arrived the 8.4V.
I cannot find these methods in its datasheet!
THANKS
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
bq24715 is a host control device and follows the host command when the battery is fully charged. So, it doesn't do the charge termination after battery is fully charged. TI battery gauge IC can report state of charge.
If you don't have a host controller to check the gauge IC and send out command, please check bq24610 charger. It has a battery termination current setting and status pin to report the battery is fully charged.