Hi Sir,
After charging termination, measure the input current less then 10mA, and the battery voltage is 4.34V, but state of CHG is still stay low(means charging).
Could you please help on this, thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
After charging termination, measure the input current less then 10mA, and the battery voltage is 4.34V, but state of CHG is still stay low(means charging).
Could you please help on this, thank you.
Hello Chentsu,
From page 23 of the datasheet: "Termination detection is disabled whenever the charge rate is reduced because of the actions of the thermal
loop, the DPPM loop, or the VIN(LOW) loop." . Please check your setup to ensure that the device isn't above 125 degrees Celsius. Also, ensure that the system load current isn't more than the preset maximum input current and Vin is not below the stated minimums.
Chentsu,
The battery voltage should not go above 4.23V. Try pulling up the CHG pin with a resistor and a LED to Out. What resistor did you change ILIM to and would you be a little more precise about the charge current after termination. Also please state the charge current during fast charge. If any of these don't help, try using a new device and see if you have the same problem.
-Raheem