Hi support!
We use a bq24123 in the charge project with 2 cells battery. There is an issure in the debugguing.The waveform between out pin of bq24123 and the inductor is similar with the another terminal of the inductor. And when the 15V ac adapter is plugged , the PG pin is low level, the voltage of the STAT1 & STAT2 is 9.2 V, voltage of VTSB is 3.2V, voltage of TS pin is 1.6V.
When the battery is existing, the BAT pin voltage is equal to the battery voltage, but there is no PWM waveform at the OUT pin.