Other Parts Discussed in Thread: CSD25402Q3A
In the BQ24171 EVM, the P-fet CSD25401Q3 is obsolete.
Is there a new updated BOM or recommended part for this design?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In the BQ24171 EVM, the P-fet CSD25401Q3 is obsolete.
Is there a new updated BOM or recommended part for this design?
3-cell Li-ion
15V DC input
1A charge, 3A total
battery charging 12.6V to 13.5V
SON3x3 I think would work and give me some headroom:
N-FET:
P-FET:
Am I on the right track?
Hi Khoi,
You only need to follow the equations on the datasheet.
ISET: ICHG= VISET/(20 x RSR)
ACSET: IDPM = VACSET/(20 x RAC)
RSR and RAC can be any value, default is 0.01ohm, but you can also use 0.02ohm or 0.04ohm if you want better accuracy at the expense of efficiency.
VISET and VACSET are selected based on the resistor divider on these pins, using VREF as reference voltage.
Regards,
Steven
Got it.
When you say better accuracy, is that in term of I_charge and I_terminate?
I'm not too concern with I-charge accuracy but the system load Rac I like it as low as possible.