I was recently trying to understand the battery charging section of a la7912 p motherboard .there in the charing section two mosfets are used are charge pumps .can you pls explain the stacked mosfets in detail thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I was recently trying to understand the battery charging section of a la7912 p motherboard .there in the charing section two mosfets are used are charge pumps .can you pls explain the stacked mosfets in detail thank you.
Wang5577 said:Varun,Charger group doesn't do the motherboard design. So, I cannot explain the design of LA7912. Where do you buy the LA7912?
I was talking about the bq24725A chip which is used inside a laptop motherboard whose board no is la7912p. There in the battery charging section bq24725a chip is used along with two stacked n channel mosfets . So the problem is i m not able to understand how exactly the mosfets along with the chip bq24725a pin 15,16,17,18,19 works to charge the battery. I detailed animated video will be verys helpful if possible. Hope you got my question now. Thanks in advance