Hello ;-),
I just want to use the bq27541-G1 in an 4S battery pack, when I read the datasheet I found a Power Supply Pin and a Battery Pin, also an LDO- so far so good , but I did not find any hint/recommanadation to connect the REGIN Pin to around 16V ( is below maximum rating ) and the BAT Pin to an potential divider - only REGIN=BAT,
is it possible to use one bq27541-G1 for a 4S Pack using different connections for REGIN and BAT ?
Thx in advance, Enrico