Hi All,
We were able to program bq27510-g2 using bqfs(generated from dfi+senc+flashstream) and our custom USB to I2C. The team is confident that the programming method and the custom USB to I2C are fully functional.
In addition, additional information needs to be appended in the golden image, specifically in the Manufacturer Block. We added this using the EV2300 and bq EVSW. The end result is the updated senc file.
We had programmed the FG using the senc file in bq EVSW and the Manufacturer Block is populated. Everything is good so far.
Using the FlashStream, we generated bqfs and dffs with psize:32.
Going back to our custom USB to I2C, we programmed the Fuel Gauge with the newly generated bqfs. Upon Reading the Data Flash, the FG had the characteristics of the DFI however, the Manufacturer Block were empty.
Is there a workaround this? How can we program using the bqfs and at the same time ensure the integrity of the Manufacturer Block is sustained?
Thanks,
Kat