How are TS faults reported on the BQ24266?
On BQ24266 datasheet page 4
TS pin5 description is: “Battery Pack NTC Monitor. Connect TS to the center tap of a resistor divider from DRV to GND. The NTC is connected from TS to GND. The TS function provides 4 thresholds for JEITA compatibility. TS faults are reported by the I2C interface. Pull TS high to VDRV to disable the TS function if unused. See the NTC Monitor section for more details on operation and selecting the resistor values”
There is no I2C interface available on the IC
How are the thermal fault reported ?