Hello all,
I am in the process of designing a 4s1p battery pack where the cells are required to be thermally isolated from each other to prevent thermal runaway in any one cell from causing a cascade effect with the other 3 cells. As such, there is no guarantee that monitoring of any one cell will give even an approximation of the temperature of the other 3 cells. Is there any method currently available to multiplex the inputs from 4 separate thermistors into the gas gauge chip?