Hi,
I am trying to charge a 3S battery pack (3,7V / 7200mAh) using self-designed hardware based on the bq40z60EVM SBS 1.1. The hardware is almost the same - i have just left out the components used for precharge. I am using the default settings for Data Memory and an AC adapter which provides 19V/4,7A.
The problem is that i can not charge the batteries - the TCA & TDA bits are set in the Battery Status register and XCHG/XDSG bits are set in Operation Status A register. I am not able to turn on the Charge FET and the Discharge FET.
I hava attached a short logfile
Regards Nermin
Wed May 13 19:05:57 CEST 2015 Device Name = bq40z60 Firmware Version = V0_13_BLD0019 Design Capacity = 7200 Design Voltage = 11100 Specification Info = 0x0031 Manufacturer Date = 1980-1-1 Serial Number = 0x0001 Manufacturer Name = Texas Instruments Device Name = bq40z60 Device Chemistry = LION Sample,DateTime,ElapsedTime,ManufAccess,RemCapAlarm,RemTimeAlarm,BattMode,@Rate(@),@TimeFull,@TimeEmpty,@RateOK,Temperature,Voltage,Current,AvgCurr,MaxErr,RSOC,ASOC,RemCap,FullChgCap,RunTimeEmty,RunTimeEmty,AvgTimeFull,ChgCurr,ChgVolt,BattStat,CycleCnt,TurboPwr,TurboCurr,SoH,OpStatA,OpStatB,TempRange,ChgStat,ChgrStat,GaugeStat,ITStat,MfgStat,SafetyAlertAB,SafetyStatAB,SafetyAlertCD,SafetyStatCD,PFAlertAB,PFStatAB,PFAlertCD,PFStatCD,CellVolt1,CellVolt2,CellVolt3,CellVolt4,vBAT,Vacp,CellCurr1,CellCurr2,CellCurr3,CellCurr4,CellPower1,CellPower2,CellPower3,CellPower4,Power,AvgPow,IntTemp,TS1Temp,TS2Temp,TS3Temp,TS4Temp,CellTemp,FETTemp,FltRemQ,FltRemE,FltFullChgQ,FltFullChgE,TrueRemQ,TrueRemE,InitialQ,InitialE,TrueFullChgQ,TrueFullChgE,T_sim,T_ambient,RaScale1,RaScale2,RaScale3,RaScale4,CompRes1,CompRes2,CompRes3,CompRes4,PackGrid,LStatus,CellGrid1,CellGrid2,CellGrid3,CellGrid4,StateTime,DOD0_1,DOD0_2,DOD0_3,DOD0_4,DOD0 Passed Q,DOD0 Passed E,DOD0 Time,DODEOC_1,DODEOC_2,DODEOC_3,DODEOC_4,QMax1,QMax2,QMax3,QMax4,QMaxDOD0_1,QMaxDOD0_2,QMaxDOD0_3,QMaxDOD0_4,QMaxPassedQ,QMaxTime,Tk,Ta,CBTime1,CBTime2,CBTime3,CBTime4,SOH_FC_Q,SOH_FC_E,ChgVoltReg,ChgCurrReg,LogRowTime(ms),LogStatus 1,2015-05-13 19:06:01,4.003,0x6110,300,10,0x6081,0,65535,65535,1,25.9,11501,0,0,100,90,42,2970,3308,65535,65535,65535,0,0,0x48C0,0,-16314,-18110,70,0x6110,0x0000,0x10,0x0004,0x0001,0xD0,0x0014,0x0618,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3822,3957,3719,0,11478,19601,0,0,0,0,0,0,0,0,0,0,32.1,25.9,25.9,25.9,25.9,25.9,32.1,2970,3196,3308,3591,2969,3195,338,395,3308,3591,25.9,25.9,1000,1000,1000,0,0,0,0,0,0,4,0,0,0,0,4027,8576,5312,9600,0,1,1,17,4512,4544,4576,0,7200,7200,7200,7200,0,0,0,0,1,17,1.0,1000,0,0,0,0,5033,5542,252,255,940,SUCCESS 2,2015-05-13 19:06:05,8.001,0x6110,300,10,0x6081,0,65535,65535,1,25.9,11501,0,0,100,90,42,2970,3308,65535,65535,65535,0,0,0x48C0,0,-16314,-18110,70,0x6110,0x0000,0x10,0x0004,0x0001,0xD0,0x0014,0x0618,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3822,3957,3719,0,11477,19599,0,0,0,0,0,0,0,0,0,0,32.0,25.9,25.8,25.9,25.9,25.9,32.0,2970,3196,3308,3591,2969,3195,338,395,3308,3591,25.9,25.9,1000,1000,1000,0,0,0,0,0,0,4,0,0,0,0,4031,8576,5312,9600,0,1,1,17,4512,4544,4576,0,7200,7200,7200,7200,0,0,0,0,1,17,1.0,1000,0,0,0,0,5033,5542,252,255,945,SUCCESS 3,2015-05-13 19:06:09,12.002,0x6110,300,10,0x6081,0,65535,65535,1,25.9,11501,0,0,100,90,42,2970,3308,65535,65535,65535,0,0,0x48C0,0,-16314,-18110,70,0x6110,0x0000,0x10,0x0004,0x0001,0xD0,0x0014,0x0618,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3822,3957,3718,0,11478,19598,0,0,0,0,0,0,0,0,0,0,32.1,25.9,25.8,25.9,25.9,25.9,32.1,2970,3196,3308,3591,2969,3195,338,395,3308,3591,25.9,25.9,1000,1000,1000,0,0,0,0,0,0,4,0,0,0,0,4035,8576,5312,9600,0,1,1,17,4512,4544,4576,0,7200,7200,7200,7200,0,0,0,0,1,17,1.0,1000,0,0,0,0,5033,5542,252,255,945,SUCCESS 4,2015-05-13 19:06:13,16.002,0x6110,300,10,0x6081,0,65535,65535,1,25.9,11501,0,0,100,90,42,2970,3308,65535,65535,65535,0,0,0x48C0,0,-16314,-18110,70,0x6110,0x0000,0x10,0x0004,0x0001,0xD0,0x0014,0x0618,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3822,3957,3715,0,11475,19601,0,0,0,0,0,0,0,0,0,0,32.1,25.9,25.9,26.0,25.9,25.9,32.1,2970,3196,3308,3591,2969,3195,338,395,3308,3591,25.9,25.9,1000,1000,1000,0,0,0,0,0,0,4,0,0,0,0,4039,8576,5312,9600,0,1,1,17,4512,4544,4576,0,7200,7200,7200,7200,0,0,0,0,1,17,1.0,1000,0,0,0,0,5033,5542,252,255,945,SUCCESS 5,2015-05-13 19:06:17,20.003,0x6110,300,10,0x6081,0,65535,65535,1,25.9,11501,0,0,100,90,42,2970,3308,65535,65535,65535,0,0,0x48C0,0,-16314,-18110,70,0x6110,0x0000,0x10,0x0004,0x0001,0xD0,0x0014,0x0618,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3822,3958,3716,0,11478,19601,0,0,0,0,0,0,0,0,0,0,32.1,25.9,25.8,26.0,25.9,26.0,32.1,2970,3196,3308,3591,2969,3195,338,395,3308,3591,25.9,25.9,1000,1000,1000,0,0,0,0,0,0,4,0,0,0,0,4043,8576,5312,9600,0,1,1,17,4512,4544,4576,0,7200,7200,7200,7200,0,0,0,0,1,17,1.0,1000,0,0,0,0,5033,5542,252,255,944,SUCCESS 6,2015-05-13 19:06:21,24.004,0x6110,300,10,0x6081,0,65535,65535,1,25.9,11501,0,0,100,90,42,2970,3308,65535,65535,65535,0,0,0x48C0,0,-16314,-18110,70,0x6110,0x0000,0x10,0x0004,0x0001,0xD0,0x0014,0x0618,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3822,3957,3718,0,11473,19600,0,0,0,0,0,0,0,0,0,0,32.1,25.9,25.9,26.0,25.9,25.9,32.1,2970,3196,3308,3591,2969,3195,338,395,3308,3591,25.9,25.9,1000,1000,1000,0,0,0,0,0,0,4,0,0,0,0,4047,8576,5312,9600,0,1,1,17,4512,4544,4576,0,7200,7200,7200,7200,0,0,0,0,1,17,1.0,1000,0,0,0,0,5033,5542,252,255,941,SUCCESS 7,2015-05-13 19:06:25,28.004,0x6110,300,10,0x6081,0,65535,65535,1,26.0,11501,0,0,100,90,42,2970,3308,65535,65535,65535,0,0,0x48C0,0,-16314,-18110,70,0x6110,0x0000,0x10,0x0004,0x0001,0xD0,0x0014,0x0618,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3822,3957,3717,0,11478,19598,0,0,0,0,0,0,0,0,0,0,32.1,25.9,25.9,25.9,25.9,25.9,32.1,2970,3196,3308,3591,2969,3195,338,395,3308,3591,25.9,25.9,1000,1000,1000,0,0,0,0,0,0,4,0,0,0,0,4051,8576,5312,9600,0,1,1,18,4512,4544,4576,0,7200,7200,7200,7200,0,0,0,0,1,18,1.0,1000,0,0,0,0,5033,5542,252,255,942,SUCCESS 8,2015-05-13 19:06:29,32.004,0x6110,300,10,0x6081,0,65535,65535,1,25.9,11500,0,0,100,90,42,2970,3308,65535,65535,65535,0,0,0x48C0,0,-16314,-18110,70,0x6110,0x0000,0x10,0x0004,0x0001,0xD0,0x0014,0x0618,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,3822,3957,3717,0,11475,19601,0,0,0,0,0,0,0,0,0,0,32.0,25.9,25.9,25.9,25.9,25.9,32.0,2970,3196,3308,3591,2969,3195,338,395,3308,3591,25.9,25.9,1000,1000,1000,0,0,0,0,0,0,4,0,0,0,0,4055,8576,5312,9600,0,1,1,18,4512,4544,4576,0,7200,7200,7200,7200,0,0,0,0,1,18,1.0,1000,0,0,0,0,5033,5542,252,255,943,SUCCESS