Hi,
i am using the BQ40Z50 with BQStudio for a BMS. First i update Firmware on Bq40Z50-R1 and do voltage calibration.
The Problem is that the gauge shows me different cell voltages than the multimeter.
All my cells have 4V but in gauge cell 2 and cell 3 have 4.4V.
Then i discharges the Pack for a new calibration but the difference is still the same. 3V Multimeter and 3.4V - 3.5V gauge.
I would like to start a leaning cycle, but if the gauge have the wrong voltages it will stop before the pack is totally charged.
What can i do to fix this problem?
Thanks for help.