In SLUSBZ5A there is Table 27 Additional Chemistry-Related Configurations:
Parameters | Li-Ion | Lead Acid | NiMH/NiCd |
Default Load Select | 1 | 3 | 3 |
Cell Term V Delta | 200 | 100 | 100 |
Min % Passed Chg for 1st Qmax | 90 | 50 | 50 |
From the dataflash of the eval board i read the following:
Load Select: 1
Cell Term V Delta: 200
Min % Passed Chg for 1st Qmax is not there. If Min PassedChr NiMH-LA 1st Qmax is meant it is: 50
I have set the Chemistry ID to 0800 (Lead Acid battery)
Load Select should be set to an appropriate value according to the Step by Step guide in the datasheet => OK.
But i have not found any information regarding the other two values. Are they set with the Chemistry ID or should/must i set them manually?