Dear, All
Customers are considering using BQ27421.
The customer has two questions.
The first is about "Figure 9. Application Schematic" in the data sheet Page 15.
In the circuit diagram, BIN PIN is connected to 2 pin of J3 via a 10 kΩ resistor.
One pin of J3 is connected to VDD and 3 pin is connected to EXT_VCC.
From here, BIN PIN seems to connect to VDD or EXT_VCC through 10 kΩ.
This does not match the explanation of the item of BIN of "Pin Functions" in the data sheet Page 3.
Please tell me the intention of the circuit diagram.
The second is about "Figure 13. bq27421-G1 Board Layout Example" of the data sheet Page 19.
Although BIN PIN is connected to VDD via Rbin, in the explanatory note it is described as pulldown with 10 kΩ.
Please tell me this intention.
Thanks, Masami M.