Other Parts Discussed in Thread: BQSTUDIO, EV2400, BQ78350, BQ76930EVM, BQ76920EVM, , BQ76940EVM, BQ76920
Hello,
recently I installed the software called BQ-Studio. So I am having a few questions about the program to get started.
Q0: As I saw, I have to configure a lot of registers in the Data memory section of BQstudio.
I would like to know if there is a default setup, which I can download somewhere and put it in BQstudio?
Q1: What is the difference between the EV2300 and the EV2400. I want to use the EV2300, are there any disadvantages, instead of using the EV2400?
Q2: In Bqustudio, there is a tab called "Firmware": Where can I download the firmware?
Thanks for help.