hello
when i open bq management softaware i dont fine qb27541 v200 i find instead qb27541 g1 which is incompatible
is there any solution for this issue?
thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello
when i open bq management softaware i dont fine qb27541 v200 i find instead qb27541 g1 which is incompatible
is there any solution for this issue?
thank you
hello onix
bq27541 G1
i have several questions please:
1-the learning cycle is succesfully completed (using batterie management software unstead of evsw) ,i used a bq27541 g1 so at least the update statues should be at 06 but it s 05 for me,is this a problem(see image update status)
2-how can i get the golden image(file.dfi)cause i have three files ".srec" ,".bq.fs" and ".df.fs" ,but no one is ".dfi "what can i do?and what is the differnace between this 3 files?(see image file)
3-i used a current tapper 50ma unstead of 175 ma , and when i finish charging i need to disconnect from the power supply but i did it after 10h,is this 2 factors the cause of dont having an update status of 06 (see image current tapper)
4-after having the golden file;i ll implement it in programming(see programming image)
hey
i ll choose directory,and then creat a golden image but i dont find a file.dfi?
helppp
hey onyx
now i have 2 quastions please:
1-when i finish charging the relax time is always 00h,i dont know why it doesnt count?
2-after finishing the learning cycle,how can i implement the golden file in other bq27541 G1?
thanx so much
hi
thank you Onyx and other
the learning cycle is finished and succefful
thank you again