This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I had the same problem whit UCD9240 + UCD7242, this is due to the current monitor of the driver that it isn't constant at temperature variation.
I solved
Does the controller throw any fault codes when it stops operating below 0C?
If there is no output there will be no PowerGood signal.
There is nothing in the FW/HW which would limit the operation at or below 0C. I would check to ensure the parts are mounted down correctly without any voids.
The values at AUXADC1 and AUXADC2 should be correct, the problem would be with AUXADC3 and AUXADC4 which are not properly initialized in the UCD9222 FW and will not return the correct values.
There is a newer FW version part which is in production but not released on the TI web yet, it is the UCD9222A controller which is compatible with the existing UCD9222. The UCD9222A returns the correct values for AUXADC3 and AUXADC4. New FW version controller's are released with a new P/N rather than as a rolling change to the existing device. Both the UCD9222 and the UCD9222A will be available moving forward.