Hello,
In my tests I have verified that if I have EXT_SYNC_IN enabled in a pwm module, the module will not produce PWM until a sync signal is present. Once the synchronization signal is provided, the PWM module operates. If the synchronization signal is removed, the PWM module keeps working at the frequency set by DPWMPRD register.
My question is this: is there an option to have the PWM module operate since the beginning even without synchronization signal? (at its own switching frequency of DPWMPRD). I have not found info regarding this feature of the PWM module not working, waiting for the sync signal.
In summary, if EXT_SYNC_IN is enabled:
- no external clock provided: DPWM does not start
- external clock provided: DPWM at external clock frequency
- external clock removed: DPWM keeps working but at its frequency defined by DPWMPRD
Is it possible to have this behavior instead:
- no external clock provided: DPWM works at its frequency defined by DPWMPRD
- external clock provided: DPWM at external clock frequency
- external clock removed: DPWM keeps working but at its frequency defined by DPWMPRD
Thank you
Marco