Hello everyone,
I am using four UCD9248 digital PWM controllers in my design to power up different rails of FPGAs DSP and ADC. To program the UCD9248 Controllers I am using TI USB-to-GPIO interface adapter EVM. The software platform which I am using is TI Fusion digital power designer.
I am facing a problem related to "SMBAlert" signal. I have programmed all the four controllers simultaneously. The controllers respond well . I have monitored the power status of all rails. The status is fine, there are no other faults appearing in the status registers except that the SMBAlert gets asserted. I have studied over the internet about the PMBus arbitration that the device with the lowest address gets the priority if multiple devices try to pull it down.Is it bad, that it gets asserted? If yes, then what should i do to remove it? Kindly help me out with this.
Thanks, Hammad.