Fusion Design Online doesn't work , what are several reasons for this case ?(hardware is OK )
thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Fusion Design Online doesn't work , what are several reasons for this case ?(hardware is OK )
thank you
Hello,
Can you install in a new folder (or remove the previous folder installed and then reinstall)? Also what is the message that is in Chinese?
Amiel
hello
I also met that question ,every time i close my software, it happens, what i can do is to install the software, is there any other solutions?
Hello,
It is unclear what is causing the problem. Can you be more specific, is the device online or offline, and is this happening with an EVM firmware from TI? The GUI will not be able to work with any firmware as it assumes a certain protocol and certain commands, if the commands are not supported in the expected way the behavior is uncertain. If you can provide more information that can help us to propose a solution.
One suggestion I may have is that if you have changed the firmware to remove support for some PMBus commands please update the command bitmask which tells the GUI which commands are supported. It may be that the bitmask is saying a command is supported and you no longer have the implementation in the firmware and the GUI tries to communicate and it causes a problem. The bitmask in the firmware is what tells the GUI what it can do with regards to PMBus.
I have tried many times ,nothing can help to do with 3.28 version. can you solve this problem in a new version?
Hello,
There are a couple topics on this thread, can you open a new one or clarify what is the problem? Sorry I'm unsure as to what issue you are referring to.