Hi,
I'm Muthu and I'm new here.
I'm using the TL1431C IC to generate 4.096V from a 5V input. The voltage divider used are R1 = 2.05 k and R2 = 3.21k. But I'm not getting 2.5V at the reference pin (8th pin). It is 2.39 V only. As per the datasheet, Vi(DEV) can go upto 20mV only.
I'm just wondering, are there any issues in the layout can make this other than IC problem? I'm getting the same issue with 4 boards. Please help.
Thanks in advance.
Regards,
Muthu