Other Parts Discussed in Thread: LM4050-N
Hi
I am looking for help with identifying differences between LM4050QAEM3-5.0/NOPB (Automotive) vs LM4050AEM3-5.0/NOPB (Industrial).
www.ti.com/lit/ds/symlink/lm4050-n.pdf
We may have to use LM4050AEM3-5.0/NOPB due to long lead times/availability of LM4050QAEM3-5.0/NOPB.
I hope these questions are correct place for this forum.
- What are differences in design?
For example: LM4050QAEM3-5.0/NOPB uses gold bond wires. LM4050AEM3-5.0/NOPB used copper bond wires.
I assume primary benefits of using gold wire in this package is more thermal cycling capability and better bonding - anything else?
Are there any other design differences?
- FIT:
Online calculator indicate same FIT/MTBF values and same sample size. Maybe it is a coincidence and that TI actually tested 2785 pieces of LM4050QAEM3-5.0/NOPB (125C Automotive) and 2785 pieces of LM4050AEM3-5.0/NOPB (125C Industrial) and 2785 piece of LM4050AIM3-5.0/NOPB (85C Industrial) in same test.
Are those FIT values product line values or values for each part number?
ELFR/DPPM values are not available online. I think those are early hour failure and/or EOL failures. HALT testing indicate 0 failures. Does missing ELFR/DPPM mean no failures observed.
My guesstimates using you calculator for DPPM at qualification temperature is 325. What is correct DDPM value?
- Temp rating
Based on "Compare all products in Shunt Voltage Reference" (see link below) both parts are available -40/125C (fixed LM4050-N and LM4050-N-Q1) .
LM4050QAEM3-5.0/NOPB is Grade 1.
It appears LM4050AEM3-5.0/NOPB is -40/125C Grade 1 part - is that correct?
- Are these two parts made on the same production line?
- Do you sort out automotive parts from the same production line?
- What is difference in EOL testing between these two part?
- How do you achieve zero defect of automotive LM4050QAEM3-5.0/NOPB (or lower defect) as compared to standard part LM4050AEM3-5.0/NOPB? Additional EOL testing, burn-in, sorting, design (Cu vs Au) etc?
- Note : LM4050AEM3-5.0/NOPB is 125C rated while LM4050AIM3-5.0/NOPB is 85C rated. What is the meaning of AEM vs AIM?
Thank you.