I used below circuit to generate +/-12V from a +5V supply. When VIN=5V/1A, VNEG=-11.7V, but VPOS=4.6V. What could be wrong?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Diaara,
Thanks for your reply. I measured below components on board.
* R3_1 = 264Kohm
* R4_1 = 119Kohm
* R11_1 = 0ohm
I don't know whether the mismatch was caused by TPS65130. Should they be close to the component values?
When ENP=3V, FBP = 0.47V. Below are the start up waveforms of INP and FBP.
CP stays at 0V during the start up.
Attached is BOM.