Hi,
I wish to use two LMG5200's cascaded, with the upper one referenced to VIN (pin1) of the lower one. Is there any reason this could lead to some issues?
Thanks,
Wouter
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I wish to use two LMG5200's cascaded, with the upper one referenced to VIN (pin1) of the lower one. Is there any reason this could lead to some issues?
Thanks,
Wouter
Hi Wouter,
there is no issue in doing this as long as you remember that the high-side LMG5200 -and all its signals- are referenced to Vin on the low-side LMG5200.
Practically this means that you will have to use a 2-channel isolator for the HI, LI inputs of the high-side LMG5200, and derive a supply that is 5V with respect to Vin of the low-side LMG5200 (by instance using an isolated supply).
Let me know if this answers your questions by clicking "very answer" below.
Best regards,
Alberto