Part Number: LMG3410
Hello,
I have a few questions regarding the LMG3410:
- The current data sheet have only typical values for most cases - how can I get the MIN,MAX values? especially for tpd,on tdelay,on trise tpd,off tfall
- I'm using the LMG3410-HB-EVM & LMG34XX-BB-EVM for evaluating the model - If I will create a situation where a shoot-through happens, will the LMG3410 protect itself, or it will burned out?
- Can you say what is the timing loss when I use a bootstrap diode for the 12V VDD? I have a 12V input voltage and I prefer using an isolated voltage for VDD - can you recommend on a specific design or part for this issue?
- What is the maximum current drawn from the VDD supply? the typical shown as 43mA.
- My main goal is to build a H-bridge topology (with 4 LMG3410) with 200V input voltage with the highest frequency - I'm aiming towards 1MHz. Is it possible for this ic? do you have a H-bridge design example?
Thank you very much,