Hello everybody!
I'm experiencing some troubles on UCC28950.
I designed a DC/DC converter able to step down a 370-410VDC PFC output voltage to a 250VDC battery pack with an insulated step down (no SR since current is low and voltage is very high, so no efficiency improvement can be achieved).
See schematic in attachment.
I'm sure to not have made mistakes (take care that the 825k resistor between SS/EN pin and GND has already been removed!), but it doesn't start!
I can observe the voltage on the SS/EN pin reach the 5V level when I pull down the DCDC_EN pin, but PWM on output are not present and also the SYNC pin doesn't run...
Any idea???
Thank you very much for your help!
Paolo0724.ZVT Control.pdf