We're using the LM25118 to produce a 12V output. When we zoom in, we're seeing some fairly large repetitive spikes at about 310kHz (I assume that's the switching frequency). They're about +/- 0.8 volts or more and are affecting the circuitry that we are powering. I understand that the LM25118 design should minimize this, and we have some large (and small) capacitors at the output to help reduce these spikes. However, since the spikes are fairly large we need to minimize them further. What suggestions do you have for doing so? Which part of the design most influences this?
The schematic is based loosely around the following web bench design (we can give the actual schematic in a separate email privately - we're including the web bench sample here):
Note that the design has an input from 9V to 36V with a 12V output. Is this an issue with us using 12V input and 12V output to test? This is a typical customer setup, so it is one that we would need to allow for. Here is a picture of the spikes that we're seeing on the output (2V per division):
Any help in correcting this would be much appreciated. Thank you.