Hello Guys,
I'm working on TPS613030 adjustable version to generate 3.3v and 5v from 2 coin cell CR2450 connected in parallel each capacity 620mAh. My peak current consumption is 320mA for the short duration of 30-40 sec. Below I'm attaching my schematic. Can you guys please review it and correct me out if there is something wrong. Also i need guidance in ferrite bead selection according to my current consumption