Dear experts,
Our assigned account is thinking of using our LM5104 device in a GaN PA Drain Switching application. The switching voltage is not a constant one but can vary between 20V to 32V. In the application, there can also be conditions to work with 250ns low pulsewidths as well as 100% duty cycle (CW) operation conditions. However, this device does not support 100% duty cycle operations like some other similar devices. So they are asking what we can suggest to work this part with 20-32V voltages and at 100% duty cycles? What would be the easiest way and with minimal PCB area?
Thanks,
Murat Ilhan.
TI-Turkey.